About BGA PAD MASK SIZE in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About BGA PAD MASK SIZE in i.MX6DQ.

Jump to solution
1,068 Views
keitanagashima
Senior Contributor I

Hi All,

Could you tell me a "BGA PAD MASK SIZE" in i.MX6DQ?

Please refer to attached detail file.

Best Regards,

Keita

Labels (2)
0 Kudos
Reply
1 Solution
972 Views
art
NXP Employee
NXP Employee

Hi Keita,

For the 0.8mm ball pitch PBGA package (as for the i.MX6Dual/Quad processors) the package-side pad mask opening diameter is equal to the pad diameter and equal to 0.4mm.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
973 Views
art
NXP Employee
NXP Employee

Hi Keita,

For the 0.8mm ball pitch PBGA package (as for the i.MX6Dual/Quad processors) the package-side pad mask opening diameter is equal to the pad diameter and equal to 0.4mm.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
972 Views
keitanagashima
Senior Contributor I

Hi Artur,

Thank you very much!

Best Regards,

Keita

0 Kudos
Reply