HID(W):LIBUSB_ERROR_TIMEOUT error while flashing IMX8MPLUS using uuu in custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HID(W):LIBUSB_ERROR_TIMEOUT error while flashing IMX8MPLUS using uuu in custom board

5,846 次查看
Cyriactoms
Contributor III

HID(W):LIBUSB_ERROR_TIMEOUT error while flashing IMX8MPLUS using uuu in custom board

I build an yocto image for IMX8mp and flashed it on custom board then encountered an error HID(W):LIBUSB_ERROR_TIMEOUT

0 项奖励
回复
21 回复数

5,616 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Have you tried to flash prebuild image for a test?

L6.6.52_2.2.0_MX8MP 

 

Regards

Harvey

0 项奖励
回复

5,607 次查看
Cyriactoms
Contributor III

yes i have tried L5.51.71 and the latest version also but i am getting the same error.

HID(W):LIBUSB_ERROR_TIMEOUT.

0 项奖励
回复

5,597 次查看
Cyriactoms
Contributor III
uuu - lsusb

uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion
==================================================
1:5 MX865 SDPS: 0x1FC9 0x0146 0x0002

0 项奖励
回复

5,591 次查看
Harvey021
NXP TechSupport
NXP TechSupport

- Try to use the new UUU tool, uuu 

- if still not work. try to add para (-v) to show more information and share your full command line

- Is the issue with one board only?

 

Regards

Harvey

0 项奖励
回复

5,584 次查看
Cyriactoms
Contributor III

sudo uuu -v -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-full-imx8mpevk.wic

uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152

Run built-in script:

uuu_version 1.4.149

# @_flash.bin | bootloader, which can extract from wic image
# @_image [_flash.bin] | wic image burn to emmc.


# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -scanterm -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mpevk-sd.bin-flash_evk -offset 0x57c00
SDPU: jump -scanlimited 0x800000
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mpevk-sd.bin-flash_evk -skipspl -scanterm -scanlimited 0x800000
SDPV: jump -scanlimited 0x800000
# }


FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all imx-image-full-imx8mpevk.wic
FB: flash -scanterm -scanlimited 0x800000 bootloader imx-boot-imx8mpevk-sd.bin-flash_evk
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done


Wait for Known USB Device Appear...
New USB Device Attached at 1:5
1:5>Start Cmd:SDPS: boot -scanterm -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000
1:5>Fail HID(W):LIBUSB_ERROR_TIMEOUT(1s)

 

I am having issue with all my custom boards.Is this a hardware issue regarding USB2.0

0 项奖励
回复

5,573 次查看
Harvey021
NXP TechSupport
NXP TechSupport

LIBUSB doesn't seem to work, as mentioned , please have a try new uuu_1.5.201 

 

Regards

Harvey

0 项奖励
回复

5,563 次查看
Cyriactoms
Contributor III
i have tried using the latest version but the same error is getting for me. Please help me to get a solution for this
0 项奖励
回复

5,541 次查看
matato
Contributor I

i.MX 8M Plus Applications Processor Reference Manual, Rev. 1, 06/2021
6.1.7 USB boot

dd.png

0 项奖励
回复

5,558 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Try with dd to flash to sd card for a test if possible for your board.

 

Regards

Harvey

 

0 项奖励
回复

5,502 次查看
Cyriactoms
Contributor III

I have done dd flash to sd card and it worked when i try to boot up i got like this

 

U-Boot SPL 2023.04-lf_v2023.04+g49b102d988 (Nov 21 2023 - 07:28:53 +0000)

DDRINFO: start DRAM init

DDRINFO: DRAM rate 4000MTS

Training FAILED

Should i need to do a ddr test before flashing.

0 项奖励
回复

5,487 次查看
gidame
Contributor III

"Training FAILED"

This result shows that what matato said is right.
matato: "Harvey, For a new custom board, should I first check whether the DDR tool can run? Am I right?"

There is something wrong with the hardware design of the DDR on this custom board.
You should run config tool to check the DDR first when you have a brand new custom board as matato said.

There should be something wrong with the layout.
Of course, it may also be that the DDR type is wrong, the difference between DDR4 and LPDDR4.
This kind of high-speed DDR4/LPDDR4 generally needs to finish SI,PI.

 

https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

das4.png

0 项奖励
回复

5,278 次查看
Cyriactoms
Contributor III

Can we do the ddr test using the config tool?
0 项奖励
回复

5,151 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Cyriactoms 

About DDR test, we'll have other engineer who will get back to you and assist on that.

 

Regards

Harvey

0 项奖励
回复

5,136 次查看
Cyriactoms
Contributor III
Please assist me on this
0 项奖励
回复

5,370 次查看
Cyriactoms
Contributor III

Download is complete
Waiting for the target board boot...
H�������������������B���݅ɕ}�����====================


********Found PMIC PCA9450**********
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:52:12
********************"************"***************************************

Waiting for board configuration from PC-end...

--Set up the MMU and enable I and D cache--

- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTB
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x97d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 0MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 4096MB
Density per controller is: 8192MB
Total density detected on the board is: 8192MB
============================================


Please re-download with the correct value

 

When i run the ddrc test  its showing like this and not able to calibrate

0 项奖励
回复

5,112 次查看
Cyriactoms
Contributor III

DDR configuration DDR type is LPDDR4 Data width: 32, bank num: 8 Row size: 17, col size: 10 One chip select is used Number of DDR controllers used on the SoC: 1 Density per chip select: 4096MB Density per controller is: 4096MB Total density detected on the board is: 4096MB ============================================ MX8M-plus: Cortex-A53 is found ************************************************************************* ============ Step 1: DDRPHY Training... ============ ---DDR 1D-Training @1600Mhz...

 

 

during calibration it is not progressing 

0 项奖励
回复

5,102 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Engineer for DDR replied back to you via other ticket, please communicate at there.

He will help you and check your configuration.

 

Regards

Harvey

0 项奖励
回复

5,294 次查看
Harvey021
NXP TechSupport
NXP TechSupport

I think that your board is i.MX8MP. Please refer to the i-MX-8M-Family-DDR-Tool-Release 

 

Regards

Harvey

0 项奖励
回复

4,745 次查看
Cyriactoms
Contributor III
i have downloaded the exact version for imx8mp
then getting this output
0 项奖励
回复

4,991 次查看
matato
Contributor I

Harvey,

 

For a new custom board, should I first check whether the DDR tool can run? Am I right?

0 项奖励
回复