Thank you for the answers Igor.
The patch is very old and didn't work :-( - but thanks for trying.
We did get the i.MX7 to work well, thank you, but we really need the GPU of the I.MX6 since we have other algorithms running.
In light of our desire to use the i.MX6, could you recommend a good 7" HDMI +USB capacitive touch screen with a resolution of 1280x720 or 1920x1080? We are searching the web for such a display now, but could use your recommendation.
You mention having a fix for 1280x960 - Could you change it to 1280x720??
https://community.nxp.com/message/819986
- +static const struct fb_videomode wvga_mode = {
+ /* 1280x960 @ 60 Hz */
+ NULL, 60, 1280, 960, 9259, 312, 96, 36, 1, 112, 3,
+ FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
+ FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, FB_MODE_IS_VESA,
+};
That would be the perfect solution for our application.
Thank you for your help!
Jonathan Tate