U-Boot 2015.04-14409-g6cf684a-dirty (Sep 19 2016 - 17:19:58)
CPU: Freescale i.MX6DL rev1.2 at 792 MHz
CPU: Temperature 48 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:1
Net: FEC [PRIME]
Error: FEC address not set.
Normal Boot
Hit any key to stop autoboot: 0
boota mmc1
kernel @ 14008000 (8398664)
ramdisk @ 15000000 (1035019)
fdt @ 14f00000 (44589)
## Booting Android Image at 0x12000000 ...
Kernel load addr 0x14008000 size 8202 KiB
Kernel command line: console=ttymxc0,115200n8 earlyprintk init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
Loading Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f0de2c
switch to ldo_bypass mode!
Starting kernel ...
I have some questions about this issue.
1. Is the step going to Kernel or Uboot ?
2. We modify the bootloader
1) uart1_pads pinmux
MX6_PAD_CSI0_DAT10__UART1_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
MX6_PAD_CSI0_DAT11__UART1_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
2) DDR 352MHz
reg 0x020C4018 value 0x000A8324
3. For imx6dl, how can I modify pinmux and DDR clock on Kernel ?