HDMI is not detecting in IMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HDMI is not detecting in IMX8QM

跳至解决方案
2,201 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

I am working on Android 9 Automotive with IMX8QM. I am using LVDS to HDMI converter to connect between BOARD and Display.

  1. Connector name is not listed under /sys/class/drm:

      ls /sys/class/drm/

         card0 card1 version

     2. dmesg | grep -i HDMI
        console=ttyLP0,115200 earlycon=lpuart32,0x5a060000,115200 androidboot.console=ttyLP0 androidboot.xen_boot=default init=/init consoleblank=0 androidboot.hardware=freescale androidboot.fbTileSupport=enable cma=800M@0x960M-0xe00M galcore.contiguousSize=33554432 androidboot.primary_display=imx-drm firmware_class.path=/ vendor/firmware transparent_hugepage=never video=HDMI-A-2:d androidboot.wificountrycode=CN

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
1 解答
1,910 次查看
vinothkumars
Senior Contributor IV

Hi, 

HDMI is working properly after flash 

"android_p9.0.0_2.1.1-auto-ga_image_8qmek2" this images instead of "android_p9.0.0_2.1.1-auto-ga_image_8qmek".

Regards,

VinothS,

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,911 次查看
vinothkumars
Senior Contributor IV

Hi, 

HDMI is working properly after flash 

"android_p9.0.0_2.1.1-auto-ga_image_8qmek2" this images instead of "android_p9.0.0_2.1.1-auto-ga_image_8qmek".

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
1,910 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi VinothS,

I’m afraid that the i.MX8QM is still on preproduction, and you need to contact with your Sales or FAE in case of requiring support.

Additionally, Android Auto is supported under “Commercial Support and Engineering Services” scheme. You could refer to the following link for additional details:

Commercial Support and Engineering Services | NXP 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复
1,910 次查看
vinothkumars
Senior Contributor IV

Thank you CarlosCasillas,

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复