HDMI Support for IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI Support for IMX6

2,900 Views
ajayvenkatakris
Contributor II

I am using the IMX6 sabre board. I have flashed the yocto-mx-sabreauto-sdcard-sd3 image using mfgtool2. The main purpose of the board is to display a video but I am not able to get any HDMI output when connected to a screen. Also after booting up, I am getting the following error.

 imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

How do I resolve this error?

0 Kudos
Reply
2 Replies

2,233 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ajay

what is full name of board, if this is Sabre SD then

mfgtool2-yocto-mx-sabresd-sdcard-sd2.vbs should be used.

Also valid kernel boot parameter should be used, please check p.14

attached Linux Guide. Use "True" HDMI display with special HDMI cable,
not HDMI - DVI adapter.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,233 Views
ajayvenkatakris
Contributor II

Board name : MX6Q-Sabreauto revA

P14 of which document should I check. Also we tried using a HDMI-VGA adapter. Would it not work that way?

Thanks

0 Kudos
Reply