Virtual node for UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Virtual node for UART

2,029 Views
deepanrajanbara
Contributor IV

Hi ,

we are using a custom board based on imx6.We wanted to know whether is it to create a virtual port for UART.Since i wanted to access a single uart for example ttymxc1 multiple times.If it is possible can you please suggest the method to do so.As am trying to communicate with our module multiple times for different purpose.

Thank you,

Deepanraj.A

0 Kudos
Reply
2 Replies

1,859 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj

please check

https://justcheckingonall.wordpress.com/2009/06/09/howto-vsp-socat/
http://stackoverflow.com/questions/52187/virtual-serial-port-for-linux

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,859 Views
deepanrajanbara
Contributor IV

Is there any third party application to create a Multiplex a single port into multiple port.In Our case we are using ttymxc1 but we need to use ttymxc1 as base port and and additional of 3 uart virtual port.

Thank you,

Deepanraj.A

0 Kudos
Reply