HABv4 vs. Advanced HAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HABv4 vs. Advanced HAB

ソリューションへジャンプ
4,445件の閲覧回数
olivergraute
Contributor III

Hello,

what exactly is the difference between HABv4 and Advanced HAB? and where do I find documentation or workshop material vor AHAB?

Best regards,

Oliver

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
4,031件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  AHAB and HAB4 documentation is available in NXP U-boot sources.

ahab\imx\doc - uboot-imx - i.MX U-Boot 

habv4\imx\doc - uboot-imx - i.MX U-Boot 

imx\doc - uboot-imx - i.MX U-Boot  

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

1 返信
4,032件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  AHAB and HAB4 documentation is available in NXP U-boot sources.

ahab\imx\doc - uboot-imx - i.MX U-Boot 

habv4\imx\doc - uboot-imx - i.MX U-Boot 

imx\doc - uboot-imx - i.MX U-Boot  

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.