HABv4 vs. Advanced HAB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HABv4 vs. Advanced HAB

Jump to solution
4,496 Views
olivergraute
Contributor III

Hello,

what exactly is the difference between HABv4 and Advanced HAB? and where do I find documentation or workshop material vor AHAB?

Best regards,

Oliver

0 Kudos
Reply
1 Solution
4,082 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  AHAB and HAB4 documentation is available in NXP U-boot sources.

ahab\imx\doc - uboot-imx - i.MX U-Boot 

habv4\imx\doc - uboot-imx - i.MX U-Boot 

imx\doc - uboot-imx - i.MX U-Boot  

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

1 Reply
4,083 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  AHAB and HAB4 documentation is available in NXP U-boot sources.

ahab\imx\doc - uboot-imx - i.MX U-Boot 

habv4\imx\doc - uboot-imx - i.MX U-Boot 

imx\doc - uboot-imx - i.MX U-Boot  

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.