Hi,
I've written an article on how to use HABv4 on i.MX6/i.MX7 to sign and encrypt your bootloader.
https://boundarydevices.com/high-assurance-boot-hab-dummies/
During my testing, I've used 4096-bit keys and everything was working fine in open mode, no HAB events. However when I closed the device it wasn't booting!
I reported the issue here already with no answer:
https://community.nxp.com/docs/DOC-330622#comment-37543
In order to boot the board with a signed bootloader I've had to add a 'Engine = CAAM' line although it was working fine in open mode with no HAB events reported! I think this should be documented somewhere.
However I couldn't get encryption to work, although, once again, it was working in open mode.
So my question: have 4096-bit keys been tested with encryption on close devices?
Looking at the HABCST_UG.pdf, it seems that a configuration for 4096 keys is provided (section 5.3.5):
Please advise.
Regards,
Gary
已解决! 转到解答。
Hi Yuri,
Thanks, it now works fine. Note this had nothing to do with the key length actually.
The problem was with the [Authenticate Data] section. It was authenticating the whole space before U-Boot entry (IVT + DCD + padding). This works in open device (no event).
But apparently when you close the device, the BootROM only copies the IVT + DCD, not the padding, hence the failure.
Regards,
Gary
Hello,
Please create request.
https://community.nxp.com/docs/DOC-329745
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------
Hi Yuri,
Isn't this support request for people that want something specific? Here I'm only asking for something that you claim in every documentation and every tutorial is working.
So it is not so much of a support request but instead a confirmation request that this feature has been tested with an explanation on how it has been verified.
Please advise.
Regards,
Gary
Hi Yuri,
Thanks, it now works fine. Note this had nothing to do with the key length actually.
The problem was with the [Authenticate Data] section. It was authenticating the whole space before U-Boot entry (IVT + DCD + padding). This works in open device (no event).
But apparently when you close the device, the BootROM only copies the IVT + DCD, not the padding, hence the failure.
Regards,
Gary
Hello Gary,
That means the (zero) padding after DCD isn't copied. This means that the authentication has to be very specific. I have few questions for you before I try them myself
Greets,
Satya
Hi Satya,
I *believe* that it means that the BootROM doesn't copy the zero padding, or at least not entirely. But at this point it is an assumption since NXP didn't comment on this.
As for your other questions:
Regards,
Gary