HABv4 - Is it possible to sign and check only a part of an image?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HABv4 - Is it possible to sign and check only a part of an image?

946 次查看
mklug_xx
Contributor I

The background of this question is as follows:

For some reasons we have a very large image (which we can't split).

Checking the whole image during secure boot would take too long.

Because CSF configuration contains start and end address, is it possible to sign and check only a part of the image?

-mk

0 项奖励
回复
1 回复

814 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, it is possible to have signed only a part of an image.

The rest of the image can be checked later if needed.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复