HABv4 - Is it possible to sign and check only a part of an image?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HABv4 - Is it possible to sign and check only a part of an image?

942 Views
mklug_xx
Contributor I

The background of this question is as follows:

For some reasons we have a very large image (which we can't split).

Checking the whole image during secure boot would take too long.

Because CSF configuration contains start and end address, is it possible to sign and check only a part of the image?

-mk

0 Kudos
Reply
1 Reply

810 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, it is possible to have signed only a part of an image.

The rest of the image can be checked later if needed.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply