HAB events with signed u-boot (wrong keys)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HAB events with signed u-boot (wrong keys)

1,059 次查看
leonardosalvato
Contributor I

Hi,

We are working on a custom u-boot for Sabre i.MX6QP using the HAB to authenticate the u-boot image. We generated the keys chain and corresponding hash. We fused the hash to the board (but didn't close the device). We tried to load a not signed image first, and the verification failed as expected. Then, we tried a signed u-boot, and there were no HAB events generated, which is fine.

Then we tried to use a different keys (all chain was generated again from scratch) for the u-boot signing but no HAB events were generated during the verification (always calling hab_status()). Do we need to close the device to see any error event?

Thank you,

Leonardo

标签 (1)
0 项奖励
回复
2 回复数

962 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request.

https://community.nxp.com/docs/DOC-329745 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you

0 项奖励
回复

962 次查看
leonardosalvato
Contributor I

Thank you very much Yuri, I'll follow official channels.

BR

Leonardo.

0 项奖励
回复