H.264 encoder Input data format support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

H.264 encoder Input data format support

跳至解决方案
2,590 次查看
ko-hey
Senior Contributor II

Hi all,

I want to know a input data format of H.264 encoder.

I 've known that i.MX8MMini support following formats.

YCbCr formats: o YCbCr 4:2:0 planar o YCbCr 4:2:0 semiplanar o YCrCb 4:2:0 semi-planar o YCbYCr 4:2:2 raster-scan
1) o CbYCrY 4:2:2 raster-scan 1)
RGB formats:1) o RGB444 and BGR444 o RGB555 and BGR555 o RGB565 and BGR565 o RGB888 and BRG888 o
RGB101010 and BRG101010

Q1.

How about i.MX8 ?

Q2.

How about i.MX8X ?

Ko-hey

0 项奖励
回复
1 解答
2,513 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot guarantee what will be the supported raw formats for the i.MX8Q and i.MX8QX until the products are completely released. What I suggest you is to test with gst-inspect-1.0 vpuenc_h264. However, this may be subject to change. There is no guarantee that it will work.

Best regards,

Diego.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,514 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot guarantee what will be the supported raw formats for the i.MX8Q and i.MX8QX until the products are completely released. What I suggest you is to test with gst-inspect-1.0 vpuenc_h264. However, this may be subject to change. There is no guarantee that it will work.

Best regards,

Diego.

0 项奖励
回复