H.264 encoder Input data format support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

H.264 encoder Input data format support

ソリューションへジャンプ
2,575件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

I want to know a input data format of H.264 encoder.

I 've known that i.MX8MMini support following formats.

YCbCr formats: o YCbCr 4:2:0 planar o YCbCr 4:2:0 semiplanar o YCrCb 4:2:0 semi-planar o YCbYCr 4:2:2 raster-scan
1) o CbYCrY 4:2:2 raster-scan 1)
RGB formats:1) o RGB444 and BGR444 o RGB555 and BGR555 o RGB565 and BGR565 o RGB888 and BRG888 o
RGB101010 and BRG101010

Q1.

How about i.MX8 ?

Q2.

How about i.MX8X ?

Ko-hey

0 件の賞賛
返信
1 解決策
2,498件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot guarantee what will be the supported raw formats for the i.MX8Q and i.MX8QX until the products are completely released. What I suggest you is to test with gst-inspect-1.0 vpuenc_h264. However, this may be subject to change. There is no guarantee that it will work.

Best regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,499件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot guarantee what will be the supported raw formats for the i.MX8Q and i.MX8QX until the products are completely released. What I suggest you is to test with gst-inspect-1.0 vpuenc_h264. However, this may be subject to change. There is no guarantee that it will work.

Best regards,

Diego.

0 件の賞賛
返信