Graphic issue with weston + qtwayland

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Graphic issue with weston + qtwayland

Jump to solution
3,366 Views
bfederau
Contributor II

Hi,

I have tested a very simple Qml app (red rectangle) with weston + qtwayland (5.4.1) on Yocto Dizzy and see now a graphic issue when resizing the window to the top or bottom of the screen.

I run the Qml app with: /usr/bin/qt5/qmlscene -platform wayland-egl test.qml

window with graphic glitch:

see attached wayland-screenshot-glitch.png

window without glitch:

see attached wayland-screenshot-no-glitch.png

The glitch doesn't appear all the time when resizing the window. After some resize steps its gone and after some more resize steps it is visible again, and so on ...

Did anybody see such a graphical issue with weston + qtwayland too?

Thanks in advanced for any feedback

-

Benjamin Federau

Tags (3)
0 Kudos
Reply
1 Solution
2,901 Views
bfederau
Contributor II

For some further testing I switched from dizzy to the master branches of oe and meta-fsl-arm layers, because I saw that there is a new vivante graphic lib version / recipe (5.0.11.p4.4+hfp) in the master of meta-fsl-arm.

With these new graphic libs the graphic issue I described above is gone now.

View solution in original post

0 Kudos
Reply
2 Replies
2,902 Views
bfederau
Contributor II

For some further testing I switched from dizzy to the master branches of oe and meta-fsl-arm layers, because I saw that there is a new vivante graphic lib version / recipe (5.0.11.p4.4+hfp) in the master of meta-fsl-arm.

With these new graphic libs the graphic issue I described above is gone now.

0 Kudos
Reply
2,901 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Benjamin,

Thanks for sharing your solution with the Community!

Best regards!

/Carlos

0 Kudos
Reply