Graphic issue with weston + qtwayland

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Graphic issue with weston + qtwayland

跳至解决方案
3,356 次查看
bfederau
Contributor II

Hi,

I have tested a very simple Qml app (red rectangle) with weston + qtwayland (5.4.1) on Yocto Dizzy and see now a graphic issue when resizing the window to the top or bottom of the screen.

I run the Qml app with: /usr/bin/qt5/qmlscene -platform wayland-egl test.qml

window with graphic glitch:

see attached wayland-screenshot-glitch.png

window without glitch:

see attached wayland-screenshot-no-glitch.png

The glitch doesn't appear all the time when resizing the window. After some resize steps its gone and after some more resize steps it is visible again, and so on ...

Did anybody see such a graphical issue with weston + qtwayland too?

Thanks in advanced for any feedback

-

Benjamin Federau

标记 (3)
0 项奖励
回复
1 解答
2,891 次查看
bfederau
Contributor II

For some further testing I switched from dizzy to the master branches of oe and meta-fsl-arm layers, because I saw that there is a new vivante graphic lib version / recipe (5.0.11.p4.4+hfp) in the master of meta-fsl-arm.

With these new graphic libs the graphic issue I described above is gone now.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,892 次查看
bfederau
Contributor II

For some further testing I switched from dizzy to the master branches of oe and meta-fsl-arm layers, because I saw that there is a new vivante graphic lib version / recipe (5.0.11.p4.4+hfp) in the master of meta-fsl-arm.

With these new graphic libs the graphic issue I described above is gone now.

0 项奖励
回复
2,891 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Benjamin,

Thanks for sharing your solution with the Community!

Best regards!

/Carlos

0 项奖励
回复