Git clone for kernel is not working ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Git clone for kernel is not working ?

1,921件の閲覧回数
robinsingh
Contributor III

Hi Guys,

I am trying to download the kernel_imx from

git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

but i am getting below error :

git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

Cloning into 'kernel_imx'...

fatal: unable to connect to git.freescale.com:

git.freescale.com[0: 192.88.156.202]: errno=Connection refused

Any idea ? is the server down ?

-Robin Singh

ラベル(3)
0 件の賞賛
返信
1 返信

1,183件の閲覧回数
saurabh206
Senior Contributor III

Hi Robin

are you working behind proxy?

You need to do proxy setting to access git.

You can also try http link.

linux-2.6-imx.git - Freescale i.MX Linux Tree

Thanks

Saurabh

0 件の賞賛
返信