Git clone for kernel is not working ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Git clone for kernel is not working ?

1,962 Views
robinsingh
Contributor III

Hi Guys,

I am trying to download the kernel_imx from

git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

but i am getting below error :

git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

Cloning into 'kernel_imx'...

fatal: unable to connect to git.freescale.com:

git.freescale.com[0: 192.88.156.202]: errno=Connection refused

Any idea ? is the server down ?

-Robin Singh

Labels (3)
0 Kudos
Reply
1 Reply

1,224 Views
saurabh206
Senior Contributor III

Hi Robin

are you working behind proxy?

You need to do proxy setting to access git.

You can also try http link.

linux-2.6-imx.git - Freescale i.MX Linux Tree

Thanks

Saurabh

0 Kudos
Reply