Git clone fail, for building kernel in the standalone

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Git clone fail, for building kernel in the standalone

跳至解决方案
1,485 次查看
mannsikchung
Contributor III

I'm trying to build Linux Kernel standalone.

But, git clone below is failing.

$ git clone http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git -b imx_4.1.15_2.0.0_ga
Cloning into 'linux-imx'...
fatal: unable to access 'http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/': Failed to connect to git.freescale.com port 80: Connection refused

The git address is from I.MX Linux User's Guide, Rev. L4.1.1.15_2.0.0_ga, 10/2016. Is the address correct?

Please share correct git address.

标签 (1)
0 项奖励
回复
1 解答
1,328 次查看
mannsikchung
Contributor III

git is working now.
Server condition is not stable.

在原帖中查看解决方案

1 回复
1,329 次查看
mannsikchung
Contributor III

git is working now.
Server condition is not stable.