Git clone fail, for building kernel in the standalone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Git clone fail, for building kernel in the standalone

ソリューションへジャンプ
2,177件の閲覧回数
mannsikchung
Contributor III

I'm trying to build Linux Kernel standalone.

But, git clone below is failing.

$ git clone http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git -b imx_4.1.15_2.0.0_ga
Cloning into 'linux-imx'...
fatal: unable to access 'http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/': Failed to connect to git.freescale.com port 80: Connection refused

The git address is from I.MX Linux User's Guide, Rev. L4.1.1.15_2.0.0_ga, 10/2016. Is the address correct?

Please share correct git address.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,020件の閲覧回数
mannsikchung
Contributor III

git is working now.
Server condition is not stable.

元の投稿で解決策を見る

1 返信
2,021件の閲覧回数
mannsikchung
Contributor III

git is working now.
Server condition is not stable.