GigE Vision camera?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GigE Vision camera?

3,637件の閲覧回数
benhenricksen
Contributor III

Has anyone used a GigE Vision camera as an input to the iMX6?

If so did you have to write a driver? Or could you just Gstreamer it as an input? Then encode using the VPU?

I know about the errata and the Ethernet bandwidth limit around 400Mbps, so it couldn't support full frame-rate HD video.

Any experience to share?

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

3,102件の閲覧回数
art
NXP Employee
NXP Employee

There is no GigE Vision standard support available for the i.MX6 series processors so far.


Have a great day,
Artur

0 件の賞賛
返信

3,102件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI benhenricksen

you are right, one can use ethernet camera, probably with smaller fps due

to erratum.

Real time 3D AVM based on 4 HD Ethernet camera at GITEX 2013, Dubai - YouTube

If GigE Vision camera can act as gstreamer server, one can use Gstreamer as an input

on i.MX6 side.

http://stackoverflow.com/questions/14890964/how-to-acquire-images-with-gige-cameras-on-linux-with-pl...

https://www.ptgrey.com/tan/10849

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------