The design file set consists of a ZIP file with artwork data, a schematic (dsn), a board file (brd), two pdfs and a bom file.
After opening the schematic in capture, an opj file is created automatically.
The the following preparatory steps seems to be needed:
- add the Layout file by right clicking on "Layout" in the file list viewer (Add Layout)
- The layout can be opened by clicking on the layout which has been added now.
Yet, some other provisions must be carried out in order to get e.g. cross probing in operation, all of them operated from the PCB main menu:
I cannot get the setup such that I can operate conveniently. For sure, it has been verified that Intertool Communication (cross probing) has been enabled, but it does not work.
Hard to believe that it is related to failing libraries, because the schematic relies on the (internal) design cache.
I´d appreciate to receive appropriate hints.