Get a Low-Power Audio sample application for M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Get a Low-Power Audio sample application for M4

ソリューションへジャンプ
2,092件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

 

I have a question about following application note.

https://www.nxp.com/docs/en/application-note/AN12195.pdf

 

One of my customer have evaluated a i.MX8MMini for their application and want to know how to control M4 core.

When they're searching some samles, they found a above note.

The control on the M4 side is similar to what my customer want to implement, so they would like to refer to it as a reference.

 

Q1.

How can we get the sample source code ?

Once we install IAR tool, can we get the code ?

 

Q2.

Which IAR tool do we need to get the code ?

 

 

Ko-hey

 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,895件の閲覧回数
art
NXP Employee
NXP Employee

The sample source code for the AN12195 application note can be found together with the application note on the i.MX8M Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-appl...

https://www.nxp.com/webapp/Download?colCode=AN12195SW

Also, the sample low power audio demo application can be found in the latest MCUXpresso SDK 2.5.0 for the i.MX8MMini CM4 core. The SDK can be configured and downloaded from here:

https://mcuxpresso.nxp.com/en/select

No IAR tool is required to use this code.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,896件の閲覧回数
art
NXP Employee
NXP Employee

The sample source code for the AN12195 application note can be found together with the application note on the i.MX8M Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-appl...

https://www.nxp.com/webapp/Download?colCode=AN12195SW

Also, the sample low power audio demo application can be found in the latest MCUXpresso SDK 2.5.0 for the i.MX8MMini CM4 core. The SDK can be configured and downloaded from here:

https://mcuxpresso.nxp.com/en/select

No IAR tool is required to use this code.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信