Get a Low-Power Audio sample application for M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Get a Low-Power Audio sample application for M4

Jump to solution
2,086 Views
ko-hey
Senior Contributor II

Hi all,

 

I have a question about following application note.

https://www.nxp.com/docs/en/application-note/AN12195.pdf

 

One of my customer have evaluated a i.MX8MMini for their application and want to know how to control M4 core.

When they're searching some samles, they found a above note.

The control on the M4 side is similar to what my customer want to implement, so they would like to refer to it as a reference.

 

Q1.

How can we get the sample source code ?

Once we install IAR tool, can we get the code ?

 

Q2.

Which IAR tool do we need to get the code ?

 

 

Ko-hey

 

0 Kudos
Reply
1 Solution
1,889 Views
art
NXP Employee
NXP Employee

The sample source code for the AN12195 application note can be found together with the application note on the i.MX8M Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-appl...

https://www.nxp.com/webapp/Download?colCode=AN12195SW

Also, the sample low power audio demo application can be found in the latest MCUXpresso SDK 2.5.0 for the i.MX8MMini CM4 core. The SDK can be configured and downloaded from here:

https://mcuxpresso.nxp.com/en/select

No IAR tool is required to use this code.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,890 Views
art
NXP Employee
NXP Employee

The sample source code for the AN12195 application note can be found together with the application note on the i.MX8M Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-appl...

https://www.nxp.com/webapp/Download?colCode=AN12195SW

Also, the sample low power audio demo application can be found in the latest MCUXpresso SDK 2.5.0 for the i.MX8MMini CM4 core. The SDK can be configured and downloaded from here:

https://mcuxpresso.nxp.com/en/select

No IAR tool is required to use this code.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply