Get Stuck at "Starting kernel ..." linux-imx6-boundary-imx_3.14.52_1.1.0_ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Get Stuck at "Starting kernel ..." linux-imx6-boundary-imx_3.14.52_1.1.0_ga

1,425 Views
sijilpu
Contributor I

Hi

I tried porting linux kernel (3.14.52) latest version on IMX.6 SABRESDB and  booted using  bootcmd command.

It shows 'Starting the kernel..after that there is no log for the rest of  kernel on serial console.

Output is :

MMC read: dev # 2, block # 2048, count 24576 ... 24576 blocks read: OK         

## Booting kernel from Legacy Image at 10800000 ...                            

   Image Name:   Linux-3.14.52                                                 

   Image Type:   ARM Linux Kernel Image (uncompressed)                         

   Data Size:    6075320 Bytes =  5.8 MB                                       

   Load Address: 10008000                                                      

   Entry Point:  10008000                                                      

   Verifying Checksum ... OK                                                   

   Loading Kernel Image ... OK                                                 

OK                                                                             

                                                                                                                        

Starting kernel ..

Steps Followed

1) Download source:

   https://github.com/boundarydevices/linux-imx6/tree/boundary-imx_3.14.52_1.1.0_ga

2) Compile the source code

   export ARCH=arm

   export CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-

   make imx_v7_defconfig

   make uImage LOADADDR=0x10008000

3) Flash Image and u-Boot to the card

   sudo dd if=u-Boot-mx6q-sabresd-no-padding.bin of=/dev/sdb bs=512 seek=2 conv=fsync  /* u-boot-sabre-boundary-imx_3.0.35_1.1.0 */

   sudo dd if=uImage_ltib of=/dev/sdb bs=512 seek=2048 conv=fsync

4) Copy complete file system from SVN to SD card.

   sudo cp -rpa [A-z]* DESTINATION FOLDER

  Is there any problems with my steps or any thing wrong with -imx6-boundary-imx_3.14.52_1.1.0_ga ?

  Could anyone guide me for this issue.

  Thanks

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

931 Views
igorpadykov
NXP Employee
NXP Employee

Hi sijil

boundary devices linux may not run on i.MX6 SABRESDB as this is different board.

Please use linux from i.MX6 product page, follow Linux Guide included in that package

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply