Generic purpose ADC iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generic purpose ADC iMX6

Jump to solution
13,481 Views
caiopereira
Contributor III

I would like to use the ADC to monitoring an analog signal in my board.

A very basic question.

How to use the ADC in iMX6?

How could I setup the adc in the device tree? Could I use the fsl,imx25-adc  driver on imx6 ?

Thank you very much

Best Regards,

Caio Pereira

Labels (2)
1 Solution
10,835 Views
igorpadykov
NXP Employee
NXP Employee

Hi Caio

only i.MX66SX,UL have ADC, test procedure can be found in

attached Linux Manual Chapter 56 ADC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
10,836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Caio

only i.MX66SX,UL have ADC, test procedure can be found in

attached Linux Manual Chapter 56 ADC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

10,835 Views
caiopereira
Contributor III

Thank you igorpadykov

0 Kudos
Reply