Generic purpose ADC iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generic purpose ADC iMX6

ソリューションへジャンプ
15,737件の閲覧回数
caiopereira
Contributor III

I would like to use the ADC to monitoring an analog signal in my board.

A very basic question.

How to use the ADC in iMX6?

How could I setup the adc in the device tree? Could I use the fsl,imx25-adc  driver on imx6 ?

Thank you very much

Best Regards,

Caio Pereira

ラベル(2)
1 解決策
13,090件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Caio

only i.MX66SX,UL have ADC, test procedure can be found in

attached Linux Manual Chapter 56 ADC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
13,091件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Caio

only i.MX66SX,UL have ADC, test procedure can be found in

attached Linux Manual Chapter 56 ADC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

13,090件の閲覧回数
caiopereira
Contributor III

Thank you igorpadykov​

0 件の賞賛
返信