Generate .sb boot loader image for imx28evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate .sb boot loader image for imx28evk

1,352 Views
sonuabraham
Contributor I

Hi ,

I am trying to build Angstrom 2016.12 based boot loader for imx28evk board. I am able to build the boot loader but the generated files are of .bin extension .

How can I request Angstrom build  system to generate .sb images which I can use with mxsldr too.

Thanks in advance.

Sonu Abraham

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,316 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sonu

nxp provides software for i.MX28EVK on

i.MX28 Evaluation Kit|NXP 

for special cases which can not be found on that page, recommended to

apply to NXP Professional Services, which helps with software customization

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply