GStreamer Pipeline for live streaming using USB Camera from imx6 board to Desktop over network

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GStreamer Pipeline for live streaming using USB Camera from imx6 board to Desktop over network

1,653 次查看
virti_choksi
Contributor III

Hello,

I want to stream a live video using USB camera connected to i.MX6 dual core board to the host system via Ethernet.

I'm using USB camera with UVC support and connected to i.MX6 dual core via USB.

The details of setup I am using are as follows:

Linux Ubuntu 18.20

Board: iMX6 dual core

USB Camera: Waveshare SBC2091

Please share the gstreamer pipeline which can be used for live streaming of the video captured by USB camera that can be used on i.MX6.

Also pipeline used on Desktop system.

Or If you can also provide the references.

My aim is to achieve the 1080p Resolution with Minimum latency lower than 30miliSec.

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,600 次查看
Dhruvit
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
Please accept my apologies for delayed answer.
 
Please find the answer below.
One can refer to these documents for the gstreamer pipeline.

GStreamer i.MX6 Camera Streaming

 
Thanks & Regards
Dhruvit Vasavda
0 项奖励
回复