GPU hangs on high temperatures

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPU hangs on high temperatures

1,735 次查看
christian_spinn
Contributor I

We're using a imx6 SoloX processor in our application. 

Temperature tests show that on high temperatures (CPU temp at 80°C) the GPU seems to hang or extrmely slow down. 

Reducing the temperature lets the GPU behave in a normal way.

Is there a known issue regarding temperature and GPU?

Is there a possibility to check GPU status, temperature and/or frequency?

Best Regards

Christian

标签 (1)
0 项奖励
回复
1 回复

1,511 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Christian,

You might have enable the thermal driver, at low temperature when reaching passive point, cooling device will lower CPU frequency and notify GPU to run at a lower frequency, check it at <Yocto_BuildDir>/linux/drivers/thermal.

imx_thermal.c, device_cooling.c   , for thermal zone driver source file

Regards

0 项奖励
回复