GPU hangs on high temperatures

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU hangs on high temperatures

1,738件の閲覧回数
christian_spinn
Contributor I

We're using a imx6 SoloX processor in our application. 

Temperature tests show that on high temperatures (CPU temp at 80°C) the GPU seems to hang or extrmely slow down. 

Reducing the temperature lets the GPU behave in a normal way.

Is there a known issue regarding temperature and GPU?

Is there a possibility to check GPU status, temperature and/or frequency?

Best Regards

Christian

ラベル(1)
0 件の賞賛
返信
1 返信

1,514件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Christian,

You might have enable the thermal driver, at low temperature when reaching passive point, cooling device will lower CPU frequency and notify GPU to run at a lower frequency, check it at <Yocto_BuildDir>/linux/drivers/thermal.

imx_thermal.c, device_cooling.c   , for thermal zone driver source file

Regards

0 件の賞賛
返信