GPU hangs on high temperatures

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPU hangs on high temperatures

1,739 Views
christian_spinn
Contributor I

We're using a imx6 SoloX processor in our application. 

Temperature tests show that on high temperatures (CPU temp at 80°C) the GPU seems to hang or extrmely slow down. 

Reducing the temperature lets the GPU behave in a normal way.

Is there a known issue regarding temperature and GPU?

Is there a possibility to check GPU status, temperature and/or frequency?

Best Regards

Christian

Labels (1)
0 Kudos
Reply
1 Reply

1,515 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Christian,

You might have enable the thermal driver, at low temperature when reaching passive point, cooling device will lower CPU frequency and notify GPU to run at a lower frequency, check it at <Yocto_BuildDir>/linux/drivers/thermal.

imx_thermal.c, device_cooling.c   , for thermal zone driver source file

Regards

0 Kudos
Reply