GPU Profiling with Vivante VDK Tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPU Profiling with Vivante VDK Tools

38,135 Views
christian_99
Contributor I

Hello,

i need to profile the GPU on an IMX6 Board. For this i got the hint to use the Vivante VDK Tools.

I build the BSP from the wiki.Wandboard.org      repo init -u https://github.com/Freescale/fsl-community-bsp-platform .

I downloaded the Vivante VDK v1.4.6 and i wanted to follow the readme.txt.

Now i have to replace the libs from the Vivante Bundle, but i exactly dont know how to.

And then the Kernel source code from the gpu driver should should be modified, but i dont kwno where i can find these files in the Yocto Project because the guide is explained how to use this for Ltib.

Have any of you got this working? I'd be most grateful for any comments / suggestions.

14 Replies

31,051 Views
abrunetto
Contributor I

Hi,

I know that this post is old but I followed i.MX_Graphics_User's_Guide.pdf seccion 7.6.2 in order to get the vProfiler and

vAnalyzer to work. I am using a i.MX6D. You have to enable the profiler at the kernel level. As someone mentioned there are several ways to do that. I used the U-Boot method, passing a kernel parameter through bootcmd:

In my case I used the following commands to achieve that:

U-boot>

env set bootargs_mmc setenv bootargs \${bootargs_base} root=/dev/mmcblk2p2 rootwait rw \${lcd} \${hdmi} galcore.gpuProfiler=1
saveenv
boot

Noticed that I just added galcore.gpuProfiler=1 to my current bootcmd variable.

You can confirmed if it worked using the following command from the shell:

cat /sys/module/galcore/parameters/gpuProfiler 

if you get a 1, it worked. 

Then you have to export the following env vars in the current session. In this case it is a X11 session, since I am going to profile an opengl application:

export VIV_PROFILE=1
export VP_OUTPUT=sample.vpd
export VP_FRAME_NUM=0
export VP_FRAME_START=0
export VP_FRAME_END=0
export VP_SYNC_MODE=0

Finally you just have to run the application and the driver will create a file called sample.vpd in the running directory.

Regards,

Ariel Brunetto

31,051 Views
sandug
Contributor I

Hi,

In case anyone does set =1 in kernel 4.1.15 bootparams and gpuProfiler does not get enabled (you get an empty vpd file), you can try replacing the value with the hex version of it, then also add showArgs, which will printout a debug message in dmesg while booting:

galcore.gpuProfiler=0x1 galcore.showArgs=0x1 

eg:

[ 2.009390] Galcore version 5.0.11.41671
[ 2.015418] Galcore options:
[ 2.021366] irqLine = 310
[ 2.028173] registerMemBase = 0x00130000
[ 2.035534] registerMemSize = 0x00004000
[ 2.039851] irqLine2D = 311
[ 2.043522] registerMemBase2D = 0x00134000
[ 2.047869] registerMemSize2D = 0x00004000
[ 2.052161] contiguousSize = 134217728
[ 2.056395] contiguousBase = 0x00000000
[ 2.060701] bankSize = 0x00000000
[ 2.065031] fastClear = -1
[ 2.068660] compression = -1
[ 2.072283] signal = 48
[ 2.075973] powerManagement = -1
[ 2.079628] baseAddress = 0x00000000
[ 2.083958] usb 1-1: New USB device found, idVendor=0424, idProduct=2534
[ 2.090714] physSize = 0x80000000
[ 2.095040] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.102219] logFileSize = 0 KB
[ 2.106090] recovery = 1
[ 2.109584] stuckDump = 0
[ 2.113076] gpuProfiler = 1

to confirm gpuProfiler variable was set to 1 and should be enabled.

Thank you all for writing all the information in this public thread, since I couldn't have done it without your help !

Best regards, Gabriel

0 Kudos
Reply

31,052 Views
jamesbone
NXP TechSupport
NXP TechSupport

Bio_TICFSL,  Can you please comment?

0 Kudos
Reply

31,052 Views
kimlim
Contributor III

It has been two months since the question is posted.

May I know is there any update regarding the Vivante GPU profiling issue?

0 Kudos
Reply

31,052 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Kim,

Please try to use the latest Linux BSP version. When building Vivante Graphics Drivers in a Linux environment, the driver is built with vProfiler capability.

To activate vProfiler functionality, there are two ways to do it:

1.       we only need to add a sentence "galcore.gpuProfiler=1" in the attribute of bootargs in your boot configuration. For example, if use the nfs to boot the linux, we can configuration boot like: setenv bootargs_nfs 'setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp video=mxcepdcfb:E060SCM,bpp=16 max17135:pass=2,vcom=-2030000 galcore.gpuProfiler=1'.

2. Use the command line to add the gpuProfiler=1 option, or add the option into an existing .sh script similar to the following:

#!/bin/bash

#

insmod /lib/modules/galcore.ko gpuProfiler=1 [OPTIONS]

chmod 777 /dev/galcore

Note: The path before file galcore.ko need not to reference this path, it is the path where your .ko file puts.


Hope this helps

31,052 Views
kimlim
Contributor III

i found that /dev/galcore is already there after i booted into my mx6 Linux BSP with or without the galcore.gpuProfiler=1.

anyway, i still configure my bootargs as follow:

setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 init=/init rootwait galcore.gpuProfiler=1'

after boot into the rootfs,i configure my environment variables as follow:

export VPROFILER_OUTPUT = sample.vpd

export VPROFILER_FRAME_NUM =100

export VPROFILER_SYNC_MODE=1

I CANT find any sample.vpd created in my directory after I run an GLES2.0 application as provided by Vivante' GPU SDK (e.g. 02_ColoredTriangle).

Any help?

0 Kudos
Reply

31,052 Views
texierp
Contributor III

Hi Kim,

I also had trouble getting the GPU profiler run.

I suggest you download this (functional) Image : backup_vProfiler.gz - Google Drive


In order to test this image, here are some commands :


1) sudo gzip -dc /path/to/backup_vProfiler.gz | dd of=/dev/sdX

2) run script in /opt

     - . ./profiler.sh

3) export VIV_PROFILE=1

4) run your application

5) put the vpd file into vAnalyser


vAnalyser.png


This is a custom distribution (LTIB)


Help :

vProfiler.pdf - Google Drive


Regards


Pierre-Jean TEXIER

31,052 Views
kimlim
Contributor III

Pierre, thanks for your useful help.

I downloaded your image and found that it can't be booted.

fdisk -l backup_vProfiler

Disk backup_vProfiler: 1948 MB, 1948254208 bytes

60 heads, 62 sectors/track, 1022 cylinders, total 3805184 sectors

Units = sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

Disk identifier: 0x00c46ff6

           Device Boot      Start         End      Blocks   Id  System

backup_vProfiler1   *           1     3801839     1900919+  83  Linux

I then used kpartx to create a mapper and mounted it

sudo kpartx -a backup_vProfiler

sudo mount -o rw /dev/mapper/loop0p1 /mnt

ls -la /mnt

total 312

drwxr-xr-x 19 root root   4096 Jan  1  1970 .

drwxr-xr-x 25 root root   4096 Sep 12 19:11 ..

-rw-r--r--  1 root root   1472 May 21 20:16 6x_bootscript

-rw-r--r--  1 root root   1483 May 20 21:24 6x_bootscript.bak

drwxr-xr-x  2 root root   4096 Jan  1  1970 bin

drwxr-xr-x  2 root root   4096 Jan  1  1970 boot

drwxr-xr-x  2 root root   4096 May 20 21:21 dev

drwxr-xr-x  6 root root   4096 Jan  1  1970 etc

-rwxr-xr-x  1 root root 214220 Jan  1  1970 galcore.ko

drwxr-xr-x  3 root root   4096 May 20 21:21 home

drwxr-xr-x  5 root root   4096 May 20 21:21 lib

drwx------  2 root root  16384 May 20 20:06 lost+found

drwxr-xr-x  7 root root   4096 May 20 21:22 mnt

drwxr-xr-x  4 root root   4096 Jan  1  1970 opt

drwxr-xr-x  2 root root   4096 May 20 21:23 proc

drwxr-xr-x  2 root root   4096 Jan  1  1970 root

drwxr-xr-x  2 root root   4096 May 20 21:23 sbin

drwxr-xr-x  2 root root   4096 May 20 21:23 sys

drwxr-xr-t  3 root root   4096 May 20 21:23 tmp

drwxr-xr-x  2 root root   4096 May 20 21:23 unit_tests

drwxr-xr-x 11 root root   4096 May 20 21:24 usr

drwxr-xr-x 11 root root   4096 May 20 21:24 var

May I know where i can obtain the linux kernel you used to boot the rootfs you have uploaded?

0 Kudos
Reply

31,051 Views
kimlim
Contributor III

i managed to load the kernel after configuring uboot with the correct boot arguments

setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw'

setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc dev 0; ext2load mmc 0:1 0x10800000 /boot/uImage; bootm'

however, it stuck at 'Waiting for root device /dev/mmcblk1p1...'

the complete boot log is as follow:

MX6Q ROM-3420 U-Boot > setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw'

MX6Q ROM-3420 U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc dev 0; ext2load mmc 0:1 0x10800000 /boot/uImage; bootm'

MX6Q ROM-3420 U-Boot > boot

mmc0 is current device

Loading file "/boot/uImage" from mmc device 0:1 (xxa1)

3799316 bytes read

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2666-gbdde708

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3799252 Bytes =  3.6 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Linux version 3.0.35-2666-gbdde708 (evu@evu-SD30V10) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #2 SMP PREEMPT Tue May 20 15:33:07 CEST 2014

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board

Ignoring unrecognised tag 0x54410008

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 194560

Kernel command line: console=ttymxc0,115200 enable_wait_mode=off video_mode=extension pcie_testmode=off root=/dev/mmcblk1p1 rootwait rw

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 512MB 256MB = 768MB total

Memory: 765956k/765956k available, 282620k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

    vmalloc : 0xc0800000 - 0xf2000000   ( 792 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x8003c000   ( 208 kB)

      .text : 0x8003c000 - 0x80a6fb28   (10447 kB)

      .data : 0x80a70000 - 0x80ad3c00   ( 399 kB)

       .bss : 0x80ad3c24 - 0x80b21acc   ( 312 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

Brought up 2 CPUs

SMP: Total of 2 processors activated (3162.11 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

bio: create slab <bio-0> at 0

mxs-dma mxs-dma-apbh: initialized

print_constraints: SPKVDD: 4200 mV

print_constraints: vmmc: 3300 mV

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

mc_pfuze 1-0008: recv failed!:-5,80

mc_pfuze: probe of 1-0008 failed with error -1

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

max17135 2-0048: PMIC MAX17135 for eInk display

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

PMU: registered new PMU device of type 0

Static Power Management for Freescale i.MX6

wait mode is disabled for i.MX6

cpaddr = c0880000 suspend_iram_base=c0918000

PM driver module loaded

IMX usb wakeup probe

add wake up source irq 75

IMX usb wakeup probe

cpu regulator mode:ldo_enable

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 1496

alg: No test for stdrng (krng)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

_regulator_get: get() with no identifier

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd

mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.3: ipu1-di0 already in use

mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

loop: module loaded

No sata disk.

m25p80 spi0.0: unrecognized JEDEC id ffffff

GPMI NAND driver registered. (IMX)

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 72

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

mousedev: PS/2 mouse device common for all mice

input: gpio-keys as /devices/platform/gpio-keys/input/input0

input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1

egalax_ts 1-0004: egalax_ts: failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

egalax_ts 2-0004: egalax_ts: failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

usb 2-1: new full speed USB device number 2 using fsl-ehci

elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20

mag3110 2-000e: check mag3110 chip ID

mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!

mag3110: probe of 2-000e failed with error -22

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!

mma8451: probe of 0-001c failed with error -22

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

Bluetooth: Generic Bluetooth USB driver ver 0.6

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA

mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

VPU initialized

mxc_asrc registered

Thermal calibration data is 0x56d4d369

Thermal sensor with ratio = 179

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

input: Logitech USB Receiver as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input2

generic-usb 0003:046D:C52E.0001: input,hidraw0: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-fsl-ehci.1-1/input0

input: Logitech USB Receiver as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.1/input/input3

generic-usb 0003:046D:C52E.0002: input,hidraw1: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-fsl-ehci.1-1/input1

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

usbcore: registered new interface driver snd-usb-audio

mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio

Cirrus Logic CS42888 ALSA SoC Codec Driver

i2c-core: driver [cs42888] using legacy suspend method

i2c-core: driver [cs42888] using legacy resume method

mmc0: new high speed DDR MMC card at address 0001

imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.

mmcblk0: mmc0:0001 M4G1FB 3.64 GiB

mmcblk0boot0: mmc0:0001 M4G1FB partition 1 1.00 MiB

mmcblk0boot1: mmc0:0001 M4G1FB partition 2 1.00 MiB

wm8962 0-001a: Failed to get supply 'DCVDD': -19

wm8962 0-001a: Failed to request supplies: -19

wm8962 0-001a: asoc: failed to probe CODEC wm8962.0-001a: -19

asoc: failed to instantiate card wm8962-audio: -19

imx_3stack asoc driver

Initialize HDMI-audio failed. Load HDMI-video first!

ALSA device list:

  No soundcards found.

NET: Registered protocol family 26

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

mmcblk0: p1

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

mmcblk0boot1: unknown partition table

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

mmcblk0boot0: unknown partition table

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

regulator_init_complete: SPKVDD: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:46:23 UTC (2783)

Waiting for root device /dev/mmcblk1p1...

0 Kudos
Reply

31,051 Views
texierp
Contributor III

Hi,

Maybe try to change "root=/dev/mmcblk1p1" by root=/dev/mmcblk0p1.


Regards

Pierre-jean

0 Kudos
Reply

31,051 Views
kimlim
Contributor III

i dd your image into an SDcard (/dev/mmcblk1p1). root=/dev/mmcblk0p1 will boot into my MX6' onboard rootfs.

0 Kudos
Reply

31,051 Views
texierp
Contributor III

Not use dd try with this command : sudo gzip -dc backup_vProfiler.gz | dd of=/dev/sdX , unzip directly on the SD Card.


Regards

0 Kudos
Reply

31,051 Views
kimlim
Contributor III

Thanks Pierre.

I think my approach should be the same with yours as I dd the result of gunzip backup_vProfiler.gz to of=/dev/sdX

0 Kudos
Reply

31,051 Views
texierp
Contributor III

Maybe yes, but I'm sure my command work :smileywink:

Keep me informed of your progress



0 Kudos
Reply