Hi,
I just wanted to set baud rate of my GNSS port to 38400 in gpsd file if anyone knows please help me.
Below is the current content of the gpsd file content
START_DAEON="true"
GPSD_OPTIONS=""
DEVICES="/dev/ttyLP3"
USBAUTO="true"
GPSD_SOCKET="/var/run/gpsd.socket"
Regards,
Brinto
Solved! Go to Solution.
Hello,
You can choose udev rule or systemd service to set baud rate before gpsd service.
Here is the udev rule:
ACTION=="add", SUBSYSTEM=="tty", KERNEL=="ttyLP3", RUN+="/bin/stty -F /dev/%k 38400"
Add rule:
udevadm control --reload
udevadm trigger --action=add --subsystem-match=tty
This should be called when ttyLP3 is detected in system.
Best Regards,
Zhiming
Hello,
Please try to add GPSD_OPTIONS="-b -s 4800"
Best Regards,
Zhiming
Got error like
Error connecting to gpsd: [Errno 104] Connection reset by peer
Regards,
Brinto
Hello,
Did you try to set 38400 baudrate and then get the log from system?
Referring the guidem, you can get the log from syslog
When gpsd is running as a daemon (not in the foreground) is sends all of its logging to syslog(3). Logging is sent with ident "gpsd" using facility "LOG_USER".
If you are using syslog-ng, then you can send all gpsd logs to a file /var/log/gpsd. Put this at the end of your /etc/syslog-ng/syslog-ng.conf file:
destination gpsdf { file("/var/log/gpsd"); }; filter f_gpsd { program("gpsd"); }; log { source(src); filter(f_gpsd); destination(gpsdf); };
Best Regards,
Zhiming
Hello,
You can choose udev rule or systemd service to set baud rate before gpsd service.
Here is the udev rule:
ACTION=="add", SUBSYSTEM=="tty", KERNEL=="ttyLP3", RUN+="/bin/stty -F /dev/%k 38400"
Add rule:
udevadm control --reload
udevadm trigger --action=add --subsystem-match=tty
This should be called when ttyLP3 is detected in system.
Best Regards,
Zhiming