GPIO read frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO read frequency

1,280件の閲覧回数
charleshuang
Senior Contributor II

Hi All,

We would like to read the GPIO triggerred by interrupt. So, we want to confirm which is the maximum frequency to read the GPIO?

We also find two articles in the community, but the information is so different.

https://community.nxp.com/thread/454951

=> It mentions 300 ns = 3333kHz.

https://community.nxp.com/message/974747

=> The picture shows it's around 4.6kHz

Best regards,

Daniel

ラベル(1)
0 件の賞賛
返信
1 返信

1,216件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

typical read gpio frequency is about several MHz however it may be slower

depending on processor loading.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信