GPIO read frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO read frequency

1,292 Views
charleshuang
Senior Contributor II

Hi All,

We would like to read the GPIO triggerred by interrupt. So, we want to confirm which is the maximum frequency to read the GPIO?

We also find two articles in the community, but the information is so different.

https://community.nxp.com/thread/454951

=> It mentions 300 ns = 3333kHz.

https://community.nxp.com/message/974747

=> The picture shows it's around 4.6kHz

Best regards,

Daniel

Labels (1)
0 Kudos
Reply
1 Reply

1,228 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

typical read gpio frequency is about several MHz however it may be slower

depending on processor loading.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply