GPIO read frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO read frequency

1,299 次查看
charleshuang
Senior Contributor II

Hi All,

We would like to read the GPIO triggerred by interrupt. So, we want to confirm which is the maximum frequency to read the GPIO?

We also find two articles in the community, but the information is so different.

https://community.nxp.com/thread/454951

=> It mentions 300 ns = 3333kHz.

https://community.nxp.com/message/974747

=> The picture shows it's around 4.6kHz

Best regards,

Daniel

标签 (1)
0 项奖励
回复
1 回复

1,235 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

typical read gpio frequency is about several MHz however it may be slower

depending on processor loading.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复