GPIO max read frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO max read frequency

ソリューションへジャンプ
2,033件の閲覧回数
Eximius
Contributor III

Hi,

We are working with a 13 bit or 9 bit parallel camera interface with clocks at 48Mhz or 24Mhz. And I would like to know what is the GPIOs max reading frequency, or if there is another interface that the camera could be directly connected to, without the needs of extra hardware.

Platform: i.MX 8M Plus

Thanks for your help.

Best regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
2,016件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi Eximius,

 

The max speed on GPIO can be found on the datasheet 3.5.1 General purpose I/O AC parameters:

nxf63675_0-1632938019088.png

And the processor has interfaces focus on a single Camera, MIPI CSI 1 can support up to 400/500 MHz pixel clock in the
Nominal/Overdrive mode.

 

Regards,

Israel.

元の投稿で解決策を見る

1 返信
2,017件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi Eximius,

 

The max speed on GPIO can be found on the datasheet 3.5.1 General purpose I/O AC parameters:

nxf63675_0-1632938019088.png

And the processor has interfaces focus on a single Camera, MIPI CSI 1 can support up to 400/500 MHz pixel clock in the
Nominal/Overdrive mode.

 

Regards,

Israel.