GPIO max read frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO max read frequency

Jump to solution
1,976 Views
Eximius
Contributor III

Hi,

We are working with a 13 bit or 9 bit parallel camera interface with clocks at 48Mhz or 24Mhz. And I would like to know what is the GPIOs max reading frequency, or if there is another interface that the camera could be directly connected to, without the needs of extra hardware.

Platform: i.MX 8M Plus

Thanks for your help.

Best regards,

Labels (1)
0 Kudos
Reply
1 Solution
1,959 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Eximius,

 

The max speed on GPIO can be found on the datasheet 3.5.1 General purpose I/O AC parameters:

nxf63675_0-1632938019088.pngnxf63675_0-1632938019088.png

And the processor has interfaces focus on a single Camera, MIPI CSI 1 can support up to 400/500 MHz pixel clock in the
Nominal/Overdrive mode.

 

Regards,

Israel.

View solution in original post

1 Reply
1,960 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Eximius,

 

The max speed on GPIO can be found on the datasheet 3.5.1 General purpose I/O AC parameters:

nxf63675_0-1632938019088.pngnxf63675_0-1632938019088.png

And the processor has interfaces focus on a single Camera, MIPI CSI 1 can support up to 400/500 MHz pixel clock in the
Nominal/Overdrive mode.

 

Regards,

Israel.