GPIO electrical AMR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO electrical AMR

1,418 Views
barakbarak
Contributor I

Hi 

I'm looking for AMR characteristisc for GPIO pins of IMX6Q.

 

Particularity I'm interested how much current can GPIO output  absorb. 

I connected the output of GPIO through resistor to another output P1, so that of P1 forces voltage it "wins" , if P1 is HighZ then GPIO forces the line. 

if P1 forces 3.3v but GPIO pulls to 0v then GPIO takeas current of 3.3V/R , what is the allowable current?

Bar.

Labels (2)
0 Kudos
Reply
1 Reply

1,313 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bar

typical current can be estimated using sect.4.8.1 GPIO Output Buffer Impedance

i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Unfortunately max. current is not specified.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply