Ft5x06 Touch Screen With Imx6q Sabre AI Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ft5x06 Touch Screen With Imx6q Sabre AI Board

558 Views
nandishguruling
Contributor III

Hello  ALL,

i am trying to interface the Ft5x06 touch (ST7789S LCD) with imx6q Sabre AI board, i am getting the interrupt signal, but touch is not working, it is very urgent task can any one help me to solve this issue, Please find the attached source files, Logs and pics, your help would be very appreciated,

Thanks in advance,

Best Regards

Nandish SG.

0 Kudos
Reply
2 Replies

440 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nandish

this part is not used with i.MX6 reference boards so unfortunately it is not possible

to validate your files. However it is used on boundary devices boards so one can look at

1280x800 displays - Boundary Devices 

or post on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

440 Views
nandishguruling
Contributor III

Hi igor

1) When I run the “lsmod” command in terminal it show the message like “ Module Size Used by” that's it

2) I googled I got some info https://community.nxp.com/thread/305927 we need to do, but where can I find the “eGalax_touch_screen.idc ” file ,

Best Regards

Nandish SG

0 Kudos
Reply