GPIO Recommendation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,308件の閲覧回数
JK-IMX
Contributor V

Hi i.MX Champ

My customer asked about GPIO with the following conditions.

Please check whan GPIO can be best choice to meet the condition below.

 

Pin : GPIO5_IO18, GPIO1_IO7, GPIO3_IO1

Condition : 

- To assign GPIO for Reset of Other Devices
- GPIO remains in a stable Pull-Up state even when i.MX 8MM is initialized or restarted.

ArrowElectronics_0-1663066733823.png

ArrowElectronics_1-1663066768315.png

ArrowElectronics_2-1663066799397.png

Please let us know what pin can be the best option to avoid glitch or unknown state during reset.

Thanks.

Regards, 

Arrow

ラベル(1)
0 件の賞賛
返信
1 解決策
2,268件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The NVCC_xxx will be pull down during reset.

Qmiller_0-1663739591801.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,261件の閲覧回数
JK-IMX
Contributor V

Hi Qmiller

Thanks for your kind answer.

Regards, 

James

0 件の賞賛
返信
2,269件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The NVCC_xxx will be pull down during reset.

Qmiller_0-1663739591801.png

 

0 件の賞賛
返信