GPIO Recommendation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Recommendation

Jump to solution
2,299 Views
JK-IMX
Contributor V

Hi i.MX Champ

My customer asked about GPIO with the following conditions.

Please check whan GPIO can be best choice to meet the condition below.

 

Pin : GPIO5_IO18, GPIO1_IO7, GPIO3_IO1

Condition : 

- To assign GPIO for Reset of Other Devices
- GPIO remains in a stable Pull-Up state even when i.MX 8MM is initialized or restarted.

ArrowElectronics_0-1663066733823.png

ArrowElectronics_1-1663066768315.png

ArrowElectronics_2-1663066799397.png

Please let us know what pin can be the best option to avoid glitch or unknown state during reset.

Thanks.

Regards, 

Arrow

Labels (1)
0 Kudos
Reply
1 Solution
2,259 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The NVCC_xxx will be pull down during reset.

Qmiller_0-1663739591801.png

 

View solution in original post

0 Kudos
Reply
2 Replies
2,252 Views
JK-IMX
Contributor V

Hi Qmiller

Thanks for your kind answer.

Regards, 

James

0 Kudos
Reply
2,260 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The NVCC_xxx will be pull down during reset.

Qmiller_0-1663739591801.png

 

0 Kudos
Reply