GPIO Pulldown IMX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPIO Pulldown IMX6SL

跳至解决方案
2,578 次查看
stephangm
Contributor I

How can I set a GPIO pin to be a pulldown without using an external resistor?

标签 (3)
0 项奖励
回复
1 解答
2,321 次查看
art
NXP Employee
NXP Employee

An internal 100kOhm pull-down resistor can be enabled on most of GPIO pins by appropriately configuring the corresponding IOMUXC_SW_PAD_CTL_PAD_<xxx> register, where <xxx> is the corresponding pin name. The sequence is as follows.

1. Set the IOMUXC_SW_PAD_CTL_PAD_<xxx>[PUS] bits to 0b00 to select the 100kOhm pull-down resistor.

2. Set the IOMUXC_SW_PAD_CTL_PAD_<xxx>[PUE] bit to 1 to enable the pull resistor (not a keeper circuit).

3. Set the IOMUXC_SW_PAD_CTL_PAD_<xxx>[PKE] bit to 1 to physically enable the pull resistor.

For more information, refer to the Chapter 30 "IOMUX Controller (IOMUXC)" of the i.MX6SoloLite Reference Manual Rev.2 document, available on the i.MX6SoloLite Documentation web page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,322 次查看
art
NXP Employee
NXP Employee

An internal 100kOhm pull-down resistor can be enabled on most of GPIO pins by appropriately configuring the corresponding IOMUXC_SW_PAD_CTL_PAD_<xxx> register, where <xxx> is the corresponding pin name. The sequence is as follows.

1. Set the IOMUXC_SW_PAD_CTL_PAD_<xxx>[PUS] bits to 0b00 to select the 100kOhm pull-down resistor.

2. Set the IOMUXC_SW_PAD_CTL_PAD_<xxx>[PUE] bit to 1 to enable the pull resistor (not a keeper circuit).

3. Set the IOMUXC_SW_PAD_CTL_PAD_<xxx>[PKE] bit to 1 to physically enable the pull resistor.

For more information, refer to the Chapter 30 "IOMUX Controller (IOMUXC)" of the i.MX6SoloLite Reference Manual Rev.2 document, available on the i.MX6SoloLite Documentation web page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,321 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Stephan,

do you want to do it in bareboard code? Modifying directly the registers? In this case you must check the Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_AUD_MCLK). Here you will find the following options for a pin:

00 100K_OHM_PD — 100K Ohm Pull Down

01 47K_OHM_PU — 47K Ohm Pull Up

10 100K_OHM_PU — 100K Ohm Pull Up

11 22K_OHM_PU — 22K Ohm Pull Up

If this is not what you are looking for please let me know details of what you need to configure so I can provide more details.


Regads,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复