GPIO Pin, Translator, LED Board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO Pin, Translator, LED Board.

4,112件の閲覧回数
MJD
Contributor III

Hi
We are controlling an LED Board using SYS_STATUS pin (GPIO3 IO16) as PWM function, LED Board control pin is in 5V power domain, so we are using two stage translator from 1.8V to 3.3V, 3.3V to 5V.

Before connecting the translator we were able to toggle the gpio pin, But after connecting with translator we are not able to do the same. How do we achieve this.?

MJD_0-1720787294200.png

 

MJD_0-1720786590195.png

 

0 件の賞賛
返信
3 返答(返信)

4,074件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MJD 

I hope you are doing well.

 

Could you please share the schematics regarding to the LED and translators?

Also, please tell me if you are trying to do it with Cortex M or Cortex A.

Also, GPIO3_IO16 has not PWM functionality on i.MX8MP, Could you please clarify.

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信

4,060件の閲覧回数
MJD
Contributor III

 

1. LED : SMD-LX0707RGB-TR

Attaching data sheet.

2. Translator: NTS0104GU12.

https://www.nxp.com/part/NTS0104GU12

 

3. GPIO3_IO16 has not PWM functionality on i.MX8MP.   Ya OK.

 

0 件の賞賛
返信

4,055件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello, 

 

Also it is helpful to take measures from GPIO to the input of the translator and output of the translator, we need to check the chain.

Also, I would like to know, what is the reason to use two translators instead of just one?

One more thing, it appears this LED is NZR communication, it is difficult to achieve from Cortex M, so, I guess you are using Cortex A? 

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信