GPIO Pin, Translator, LED Board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Pin, Translator, LED Board.

4,242 Views
MJD
Contributor III

Hi
We are controlling an LED Board using SYS_STATUS pin (GPIO3 IO16) as PWM function, LED Board control pin is in 5V power domain, so we are using two stage translator from 1.8V to 3.3V, 3.3V to 5V.

Before connecting the translator we were able to toggle the gpio pin, But after connecting with translator we are not able to do the same. How do we achieve this.?

MJD_0-1720787294200.png

 

MJD_0-1720786590195.png

 

0 Kudos
Reply
3 Replies

4,204 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MJD 

I hope you are doing well.

 

Could you please share the schematics regarding to the LED and translators?

Also, please tell me if you are trying to do it with Cortex M or Cortex A.

Also, GPIO3_IO16 has not PWM functionality on i.MX8MP, Could you please clarify.

 

Best regards,

--... ...--

Salas.

0 Kudos
Reply

4,190 Views
MJD
Contributor III

 

1. LED : SMD-LX0707RGB-TR

Attaching data sheet.

2. Translator: NTS0104GU12.

https://www.nxp.com/part/NTS0104GU12

 

3. GPIO3_IO16 has not PWM functionality on i.MX8MP.   Ya OK.

 

0 Kudos
Reply

4,185 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello, 

 

Also it is helpful to take measures from GPIO to the input of the translator and output of the translator, we need to check the chain.

Also, I would like to know, what is the reason to use two translators instead of just one?

One more thing, it appears this LED is NZR communication, it is difficult to achieve from Cortex M, so, I guess you are using Cortex A? 

 

Best regards,

--... ...--

Salas.

0 Kudos
Reply