GPIO DC/AC timing parameters in Schmitt trigger mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO DC/AC timing parameters in Schmitt trigger mode

1,845 次查看
ko-hey
Senior Contributor II

Hi all

I have question about GPIO specification.

I doubt that the DC/AC timing parameters are different.

Because the behavior is different in CMOS mode and Schmitt trigger mode in my board.

So I want to confirm the following.

1.

Does the DC parameter that is shown in P39 of IMX6SDLAEC is for CMOS mode ?

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf

2.

Are there any different DC and AC parameter in CMOS mode and schmitt trigger mode ?

3.

In my understanding, i.MX becomes slower to recognize a "high" level in schmitt trigger mode than CMOS mode.

Because of the delay, is there possibility that i.MX can't latch the data correctly ?

ko-hey

标签 (1)
0 项奖励
回复
3 回复数

1,688 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

1. yes

2. with schmitt input hysteresis enabled, trigger may be later than

without hysteresis, because additional time is needed for signal

to reach hysteresis level. For example without hysteresis enabled

typical trigger level 0.5*OVDD, with hysteresis enabled it will be

0.5*OVDD + hysteresis value. According to Footnote 3 :

Hysteresis of 250 mV is guaranteed over all operating conditions when hysteresis is enabled.

3. yes this is correct understanding.

>Because of the delay, is there possibility that i.MX can't latch the data correctly ?

no.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,688 次查看
ko-hey
Senior Contributor II

Hi Igor

Let me confirm about question No.3.

You mean that i.MX may fail latching a data.

Is it correct ?

ko-hey

0 项奖励
回复

1,688 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

no, meaning that i.MX will not fail latching a data.

Best regards

igor

0 项奖励
回复