GPC/GPT Sync Issue ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPC/GPT Sync Issue ?

2,356 Views
harish_g
Contributor III

While i was digging through the source code of various other examples in FreeRTOS BSP provided by NXP , i found that 2 programs , low_power_imx7d and gpt.c driver file . Similarity between these two files is that , they both use GPT for providing delays . Eventhough blinking_imx_demo uses GPT , like i mentioned in another question , it hangs whenever linux boots .But these 2 programs produced binaries which worked even after linux boots . The only difference that has any connection with GPTs between the working and the not-working programs was the use of an additional timer ( GPTB ) in this case . Eventhough , there is absolutely no use for GPTB in the flow of low_power_imx7d demo , they have still assigned clocks for GPTB . The source code snippet is the one i found .

/* In this demo, we need GPT4 to work as a patch to fix GPC sync issue */ 
RDC_SetPdapAccess(RDC, BOARD_GPTB_RDC_PDAP, 3 << (BOARD_DOMAIN_ID * 2), false, false); 
/* Select GPTB clock derived from OSC24M */ 
CCM_UpdateRoot(CCM, BOARD_GPTB_CCM_ROOT, ccmRootmuxGptOsc24m, 0, 0);
 /* Enable clock used by GPTB */ 
CCM_EnableRoot(CCM, BOARD_GPTB_CCM_ROOT); 
CCM_ControlGate(CCM, BOARD_GPTB_CCM_CCGR, ccmClockNeededAll);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

What did they mean by 

we need GPT4 to work as a patch to fix GPC sync issue

Is there any dependence issue between GPTA and GPTB ? Or is this part of some other issue ?

Regards ,

G.Harish

Labels (1)
0 Kudos
Reply
1 Reply

2,145 Views
igorpadykov
NXP Employee
NXP Employee

Hi harish

seems it is used for issue for "TO1.1" chips (simiar to "ERR007265" in i.MX6 )

and described in attached lpm_mcore.c.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply