Fusion 7' touchscreen not initialized correctly on imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fusion 7' touchscreen not initialized correctly on imx6q

1,175 Views
nxpsri
Contributor II

I'm seeing the following fusion-ts driver error during 4.14.98 Linux kernel bootup on imx6 SoM :

OF: /soc/aips-bus@02100000/i2c@021a0000/touch@0x10: could not get #reset-cells for /soc/aips-bus@02000000/gpio@020b0000

with the following device tree following GPIO Reset controller 

 

/
{
	fusion_reset: reset-controller {
		compatible = "gpio-reset";
		reset-gpios = <&gpio6 2 GPIO_ACTIVE_HIGH>;
		reset-delay-us = <10000>;
		#reset-cells = <0>;
	};
};

&i2c1 {		
	status = "okay";
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c1_mercury
			&pinctrl_touch_mercury>;

    fusion_touch: touch@0x10{
		compatible = "fusion-ts";
		reg = <0x10>;
		interrupts-extended = <&gpio7 12 IRQ_TYPE_EDGE_RISING>; 
		resets = <&fusion_reset>;
		//status = "okay";
	};
}; 
&fusion_touch {
	status = "okay";
};

 

 

Any pointers on what's going on here?

Labels (2)
0 Kudos
Reply
1 Reply

1,161 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello nxpsri,

 

You must be using the I2C in another instance since there's no error in your device tree, what error do you see in your console?

Regards

 

0 Kudos
Reply